Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
GaN-Power-Slide7

Pictured here is the system efficiency of a 12V input to 1.2V output buck converter using the 30 V EPC2100. At 500kHz the peak efficiency reaches a record-making 93%. The system clocks in at over 91% at 1MHz. Since these half bridges were built for speed, this presentation will look at even higher frequencies.

PTM Veröffentlicht am: