Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
TVS-Slide10

CeraDiode’s millions of p-n junctions offer greatly improved reliability as compared to silicon based devices. Also, CeraDiodes do not require derating until 85°C as compared to 25°C for silicon diodes. This allows them to offer higher levels of ESD protection even at elevated temperatures.

PTM Veröffentlicht am: