Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
J10X-Slide8

When going into the high-resistance state, the PTC ceramic limits its energy absorption to a non-critical value, whereas the fixed ohmic resistor shows a linear rise of the absorbed energy. In the example, the fixed resistor must have a rated power of above 200 W in order to avoid overheating and subsequent destruction.

PTM Veröffentlicht am: