Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
current-sense-slide16

In summary, CSTs are used for controlling and protecting circuits as well as detecting loads in power supplies. EPCOS has two new CST series suited for compact DC/DC converters which feature integrated primary winding, space-saving design, and transfer ratios from 1:20 to 1:125. The first series is compatible with existing designed based on an EE5 core and the second series was developed with a much smaller E4.2 core.

PTM Veröffentlicht am: