Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
SMD-Disk-Slide4

The chart on this slide illustrates the main differences between the three CU varistor case sizes as well as their associated disk diameters. Additionally, the main electrical parameters of each CU type, the dimensions of the plastic case sizes, and a cut away view showing the basic construction of the SMD CU varistor component are shown. Also shown are the rated AC voltages, the surge current ratings, and the energy absorption rating of each CU type.

PTM Veröffentlicht am: