Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
switching-regulator-slide13

Looking deeper at control loop theory for switching regulators, the above plot shows the open loop response of a switching regulator. The error amplifier has been removed, and simply perturbing the control signal into the modulator, the modulator has some gain. In this case it’s a little bit more than 20 dB, and included is the response of the LC filter on the output. There is a double pole at the LC double pole frequency, and then there’s an ESR zero. For a switching regulator 20dB of gain is not enough to provide good line and load regulation, so an error amplifier needs to be added to increase DC gain.

PTM Veröffentlicht am: