Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
digital-control-slide6

So in the digital compensator, shown here in the s domain, the designer only has 2 poles and 2 zeros rather than the classical type 3 compensation normally used in a voltage mode controller. This is because in actuality, the high frequency pole, here omega P 1, is actually a complex pole that can not be mapped to the s domain. The implications of this will be looked at later.

PTM Veröffentlicht am: