Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
Image of Flexxon X-PHY® M.2 2280 SSD - Operation Flow for Windows

By default, the security settings are disabled. Users will have to access the Windows application tool when it is first powered on, setup the email and password, and configure the Google/Microsoft authenticator. Security settings can be configured based on the required detection. Enter OTP to confirm the change. Once a security event occurs, the SSD will be locked. If physical attack and wipe data is enabled, the data will be purged from the SSD physical block.

PTM Veröffentlicht am: