Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
sw bytes
It is worth noting that although the physical interfaces support up to 32-bit wide data, the driver API operates on the basis of buffers of data bytes (8-bit). This slide defines how a byte in the user’s application buffer will relate to their physical pins. The first byte relates to pins 7-0, the second byte relates to pins 15-8, the third byte relates to pins 23-16, the fourth byte relates to pins 31-24, and the fifth byte relates to pins 7-0.
PTM Veröffentlicht am: