Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
DIN-Power-Slide12

In summary, DIN Power connectors affirm HARTING’s position as a leader in DIN 41 612 connectivity by further extending the capability detailed in module 1 of this training (DIN Signal). Standardized power solutions in 6A and 15A types are further enhanced with the complementary types, including mixed configurations. In addition to traditional wave soldering, press -in and SMC offer significant benefits in the processing of connectors and boards. Solutions for the rail transportation market have led to the DIN Power range becoming widely adopted throughout the rail industry due to the robust design and market specific variants. Customer specific contact loadings offer easy customization for both partially loaded and hot swap (first mate/last break) requirements. The combined benefits of standard and complementary types ensure that DIN 41 612 connectors will continue to provide robust and reliable connectivity solutions for system designs well into the future.

PTM Veröffentlicht am: