Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
har-modular® Configurator

Thanks to an online configurator, it is easy to select modules to create the required connector configuration. Assembly of the modules is quick and easy, as locking strips ensure that the modules align correctly and precisely. The assembled connectors can be disassembled and the modules repositioned if required. This represents an enormous simplification of work and time savings on the way to deciding on the finished configuration. True to the claim of "create their own", users can choose from a selection of modules with contacts for power up to 40 A, signal, and coaxial. The choice of metal or plastic guide pins provides precise alignment during mating. Once a desired configuration is selected, the user can request assembled connectors from HARTING.

PTM Veröffentlicht am: