Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
micro-coaxial-slide2

The series that will be reviewed in this training module are the DF81 series which is a 0.4mm pitch connector with a mated height of 0.9mm. The DF80 series which has a 0.5mm pitch and 1.72mm mated height, the DF36 and DF36A which both have a 0.4mm pitch and 1.5mm mating height.

PTM Veröffentlicht am: