Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
w.fl-slide6

This chart illustrates the V.S.W.R and insertion loss values for both the 0.81mm and 1.0mm diameter cables over frequency ranges from 0 to 6GHz, using 100mm long cables. Typically, cable sizes will be determined by the performance requirements needed from the assembly or device. For inspection purposes, Hirose offers SMA to W.FL conversion adaptors for testing of cables and receptacles. 

PTM Veröffentlicht am: