Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
i2c

Next, identify if the board is an I2C or SPI MicroPressure evaluation board. If the designer has an I2C sensor, one will need four jumpers to make four connections. First, connect the SDA of J9 on the SEK002 to the SDA of the MPR breakout board. Next, connect the SCL of J8 on the SEK002 to the SCL of the MPR breakout board. Finally, apply power by connecting the 3V3 and GND from the evaluation board to the matching headers on the SEK002.

PTM Veröffentlicht am: