Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
Clock-Slide10

The advantage of a silicon clock synthesizer is not limited to the higher level of integration over discrete components. Silicon clock synthesizers offer the flexibility of generating many output frequencies from any input frequency at any voltage. Clocks can be turned on or off using an output enable or power-down pin, and frequencies can be changed on the fly. In addition, spread spectrum modulation can be added to any clock to reduce EMI in the system.

PTM Veröffentlicht am: