Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
Software Development Platform

This slide will discuss one of HX3’s values, which is a full configuration of a communication channel with an easy-to-use programming tool, the HX3 Blaster Plus. HX3 can read, erase, and configure data of the EEPROM. Custom firmware is downloadable from a PC and can be stored on the EEPROM. It is also capable of sending data over EEPROM in the host mode configuration. If the customer wants to know more about the evaluation kit for programming with HX3 Blaster Plus, more information can be found on Infineon's product webpage. There, the customer can download the setup file and install a Blaster Plus tool kit on their PC. User guides, application notes, and datasheets are also available.

PTM Veröffentlicht am: