Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Discrete Power MOSFETs 40V and Below Slide 15
In summary, for low voltage market, there are mainly two types of applications, DC-DC switching and DC applications. In a DC-DC application, Vout is not equal to Vin. It could be a step up or step down conversion; however, most of the cases are step down conversion, which means Vout will be less than Vin. A DC application is used for load switch, OR-ing and battery management. In these types of application, Vout is ideally equal to Vin and current is continuously flowing or not at all, like a lamp switch.
PTM Veröffentlicht am: