The 10120 series from IRISO has four distinct product features to solve many common issues with connectors in harsh environments, such as those in the automotive market. The first product feature is IRISO’s proprietary Z-Move™ technology that uses a spring feature that allows for free movement in the X,Y, and Z directions. This added movement helps absorb surface vibrations caused by harsh operating conditions. This series is one of IRISO’s most space-saving floating connectors. The “floating” feature prevents mated terminals from moving, which in turn helps to avoid fretting of the contacts. The floating feature also helps the connector to self-align, which helps prevent stress on the solder joints.