Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
MLCC-Slide10

Voltage Coefficient of Capacitance describes change of capacitance vs DC voltage applied. This is a property of ceramic materials and applies to all manufacturers. The graph shows typical voltage coefficient curves for 500VDC rated X7R and NP0 capacitors. Note that the capacitance of the NP0 remains stable with applied voltage, while the X7R material can have a capacitance loss of 80% at rated voltage.

PTM Veröffentlicht am: