Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
Applications

In regards to applications, the range of where the Flex Suppressor® can be used for improving the quality of RFID communication is expanding exponentially. Mobile phones, laptops, and tablets are of course the forerunners. However, as the environment is getting further connected, smarter, and requiring more and more touchless possibilities, RFID card readers and writers, RFID cards, and tags are continuously in demand for communication distance enhancements. Most of these applications have very tight space availabilities, and this is where the Flex Suppressor comes in handy, as it can be cut into any shape. For ease of RFID tag production, the roll type of the M4 series mentioned in the previous slide can be laminated directly to the tag roll, as shown here on the right.

PTM Veröffentlicht am: