Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Example Buck Converter (cont’d.)

Shown here in the upper left is the inductance formula for a buck regulator with the maximum input voltage of 36 V, which yields a 40.44 µH inductor at 1 A. Using the KEMET METCOM MPX series listed at the bottom, a designer can use the 47 µH inductor with a saturation current of 2.5 A. The saturation current is defined as 20% decrease in inductance value at a rated current. Looking at the graph in the upper right with an output current of 1 A and an inductance above 40 µH, the designer can use the 47 µH part highlighted.

PTM Veröffentlicht am: