Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Pyroelectric Infrared Sensor

Pyroelectricity can be described as the ability of certain materials to generate a temporary voltage when they are heated or cooled. The pyroelectric sensor uses the pyroelectric effect of ceramics to detect infrared energy from a human body. It is important to note that the sensor detects a heat source if there is more than a 4°C temperature difference from ambient temperature. This means it can also detect spot light and sunshine if there is enough of a temperature difference.

PTM Veröffentlicht am: