Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Product List
Image of Kingston Technology SSD Interface Comparison: SATA vs. NVMe - Introduction

Welcome to the Kingston Technology SSD Interface Comparison: SATA vs. NVMe product training module. This presentation will help designers and engineers understand the difference between a SATA SSD and an NVMe SSD, along with some of the different form factors. When it comes to superior storage technology, NVMe is in a league of its own. Even at a glance, the differences between NVMe and SATA in performance are impressive. The communication drivers and interface between NVMe and SATA are completely different as SATA uses AHCI drivers that are designed for hard disk drives with spinning technology, while the NVMe driver is specifically designed for SSDs with Flash technology. In addition, NVMe can take advantage of the PCIe sockets to communicate between the storage interface and system’s CPU for even greater leverage. If this matchup were a sporting event, it would be like comparing an F1 race versus a super touring race. While they are both fast, comparing these two types of solid-state drives highlights their differences.

PTM Veröffentlicht am: