Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
LT3652-Slide4

The LT3652’s innovative input voltage regulation control loop extracts the maximum available power from the solar panel, reduces charge current if the panel output voltage falls below a programmed level, maintains the panel at the output voltage corresponding to the peak output power point for the particular solar panel being used, and programs the specific desired peak-power voltage via a resistor divider.

PTM Veröffentlicht am: