Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
LT3081-Slide3

Safe operating area is the power handing capability of a power transistor over voltage and current conditions. Alternatively, it is also a measure of the power transistor’s robustness or ruggedness in how much power it can handle without requiring current limit to be decreased. A wider safe operating area means that the power transistor can output higher current at high VIN-VOUT conditions. It has less current limit foldback.

PTM Veröffentlicht am: