Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
LTPoE-Slide6

Minimizing heat can be especially challenging at higher power levels. Linear Technology’s latest generation of PoE controllers use external key components whenever applicable. For PSEs, this means using external low RDS(ON) MOSFETs and 0.25 Ω sense resistors. For PDs, an external low RDS(ON) MOSFET also maximizes the amount of power delivered to the load. Not only can the user size components per the application’s heating and efficiency requirements, but they can also focus their thermal dissipation efforts on the sources of heat rather than the entire PSE or PD controller. For multi-port PSEs, external MOSFETs also provide increased reliability since adjacent ports will be unaffected by a port with a damaged or nonfunctional MOSFET.

PTM Veröffentlicht am: