Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
HighPower-TVS-Slide10

When designing for AC systems, remember that the peak voltages are much higher than the commonly used RMS voltages. It must also be understood whether it is designed for phase to neutral or phase to phase protection as that also affects the peak voltages. Choosing a VR (Reverse Voltage) that is even slightly too low can lead to overheating of the TVS diode due to continuous power dissipation.

PTM Veröffentlicht am: