Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
Summary

In summary, Littelfuse's SPDs are designed for equipment protection from transient overvoltage events. SPDs look to limit the overvoltage surges that can occur in sub-distribution boards where sensitive equipment is stored. These devices are offered in multiple pole versions for all types of distribution systems. SPDs reduce surge voltages to a level that the power distribution system and the equipment that is connected to the system can handle. SPDs protect the programmable logic controller in the equipment that they are building: power supplies, the step-down transformer, variable-frequency drives, and the input/output devices. SPDs are primarily rated by how much of a surge current magnitude they can handle and how well they limit the voltage when conducting that surge current. They are not one-size-fits-all devices, nor do the size of their kA rating (the surge rating) go hand-in-hand with the size of the panel. In other words, do not select an SPD with a maximum kA rating just because the panel is large.

PTM Veröffentlicht am: