Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
LED-slide6

The actual construction of an LED is very simple. An LED begins with the semi-conductor chip located in the center of the lead frame reflector cap. The entire chip is enclosed within either a clear or colored epoxy encasement, thereby making the LED nearly indestructible. The LED is then set into a assembling package for mounting on a circuit board in either a through-hole or surface-mount construction.

PTM Veröffentlicht am: