Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
MAX-Slide11

In summary, the new Analog DevicesnanoPower MAX1722x series of low power boost converters with True Shutdown™ consumes less than 1µA of current in the quiescent state. It will also double the battery life of wearable or health monitoring devices, and can reduce the solution size by 50% and offer up to 95% accuracy.

PTM Veröffentlicht am: