Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
Sub system
The MAX34417 can be used in any system where power needs to be monitored. Shown here is a general subsystem block diagram for a tablet. A laptop may have a similar block diagram. The heart of the system is the processor, in this case an Intel i7. The processor is surrounded by all the peripherals. The MAX34417 monitors the rails of any of these peripherals. For example, in this case, the wireless connectivity IC, touchpad, Microprocessor, battery, SSD, camera, sensors, and another storage device are being monitored by the device. Additional 34417s can also be added to monitor additional peripherals. The only limits are cost and space.
PTM Veröffentlicht am: