Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
1 wire
The DS2484 is the platform used for Analog Devices' 1-wire hardware master with adjustable timing and sleep mode. The 1-wire supports bit-banging to allow a different connection format to the master. With a 1-wire master there is ultimate reliability in the readings from the engineer’s data. It can support a range of 100 m, which is ideal for a single room. Do not forget that the engineer can use multi-drop for up to one hundred MAXREFDES131 boards to monitor multiple rooms. This also supports the Grid-EYE at ten frames per second bit rate, for the highest communication data rate.
PTM Veröffentlicht am: