Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
LCC-Slide13

The LCD Explorer development board is a 8-Common LCD board for evaluation of the PIC24F and PIC18F LCD devices. The board comes with the PIC24FJ128GA310 PIM and supports Microchip’s 100-pin microcontrollers with x8 common Segment LCD Drivers. The LCD Explorer provides an ideal platform for a customer to evaluate a MCU with a x8 Common LCD Driver on a 38 segment x 8 common LCD display. The board has a PICtail plus connector to permit PICtail plus daughter cards to be utilized, allowing development of other functions such as wireless connectivity. There is a CTMU switch on the board to showcase touch sensing. The VBAT battery back up feature allows for RTCC to run on VBAT during VDD loss.

PTM Veröffentlicht am: