Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Pt2-Slide4

The UART module has three additional features. First is full hardware support for the LIN bus protocol. In dsPIC30, significant software overhead is required to implement some of the LIN bus features. In dsPIC33, hardware in the UART module takes care of the autobaud detection and break character generation. Second, is IRDA infrared communication protocol support. The encoder/decoder and polarity control for the infrared emitter and detectors are included in the UART hardware. Third, higher baud rates are achievable by providing an additional baud clock generation mode that is 4 times faster than the divide by 16 clock mode available on the dsPIC30.

PTM Veröffentlicht am: