Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
MCP3901-Slide10

In addition to being SPI compatible, the MCP3901 has an addressable SPI interface to make easier the communication between multiple MCP3901 devices. This is particularly useful in multi-phase energy measurement applications. For industrial applications using ratiometric sensors, the differential internal voltage reference is very useful.

PTM Veröffentlicht am: