Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
Heavy Duty Rectangular Connectors Slide 4

The Molex GWconnect Heavy-Duty Connector Solution is comprised of 4 main components. The first of those components is the Housing. The Housing enclosure is stationary and would typically be mounted to the machinery or panel equipment. It is available in a surface mount style with one or two entry points as well as a bulkhead mounting style where the wire connections would come up from inside of the equipment it is mounted on. The image shown here on the bottom left shows a bulkhead mounted style Housing while the image on the right shows a surface mount style Housing with two threaded entry points. The Housing will normally have one or two latching levers, however it is also available with pegs in a reverse latching system where the latching levers are located on the Hood Enclosure. The Housing image on the right is an example of a reversed double latching system with 4 pegs. The Molex GWconnect line of Heavy-Duty Rectangular Housings are compatible with various competitor inserts for easy replacement.

PTM Veröffentlicht am: