Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
Permaseal-Slide5

Molex has the widest range of splices available from 22AWG, all the way up to 8AWG. Very few manufacturers offer an 8AWG splice. Molex also offers step-down versions of the Perma-Seal™ splice which can join two different wire gauges. This is a very unique splice which is offered by Molex but is not widely available from other manufacturers.

PTM Veröffentlicht am: