Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
ferrite class
When a designer shops for a ferrite bead for a particular EMI suppression application, typically the specification of primary interest is the component’s Impedance vs. Frequency characteristic. Most bead manufacturers will specify this value at the commonly accepted reference frequency of 100 MHz, and supplement this “one-point” spec with a typical curve showing the variation of “Z” (Impedance) vs. “f” (frequency) for a particular bead in question. With so many characteristics available for so many different applications, it can sometimes be difficult to quickly determine the best choice for a given situation. Murata’s offerings can be broadly grouped into five major areas, depending on the intended application. The resulting shape of the Z/f curve is determined by both the ferrite formulation and the geometry of the internal electrode structure.
PTM Veröffentlicht am: