Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
Posistor-Slide12

This figure shows a selection guide of the PRF series. Consider the temperature difference between the heat source and the thermistor’s location when selecting the appropriate thermistor part. The available range of sensing temperatures, are from 65°C to 145°C, in 10°C steps. The sensing temperature is specified at 4.7 kOhm and it’s also specified at 47 kOhm when the higher gain is required.

PTM Veröffentlicht am: