Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
PAEC-Slide22

The ECAS series is RoHS compliant and rated at MSL 3. It is shipped in moisture-proof packaging and can be stored under normal warehouse conditions. The capacitors should be kept dry using desiccators or other methods after unsealing the moisture-proof packaging. If more than 2 weeks has passed under the designated storage environment specified in the spec after unsealing the packaging, it is recommended that voltage should be applied and baked under said conditions.

PTM Veröffentlicht am: