Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
T9-Slide4

The two pictures here show: the majority of low voltage MOSFET competitors use a platform called a split gate technology and Nexperia uses a unique low voltage super-junction approach. As can be seen here, the split gate approach has a narrower cell pitch than Nexperia’s super-junction approach. This is important in terms of avalanche capability explained on the next slide. To note: other competitors have super-junction technology, but for higher voltages, such as 500V-1000V, Nexperia is the only one to have it at low voltage 40V in T9.

PTM Veröffentlicht am: