Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Gender Options

All VULCON connectors are available in both gender options. This is a design decision at the engineering level and depends on the end use application. Usually females are preferred on the panel/box side to meet UL and other agency requirements. In more rugged applications, it may be preferable to have the male on the panel/box side with a female external cable eliminating moisture and contamination build-up at the panel/box.

PTM Veröffentlicht am: