Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
summary
In this course, you learned about the LPC2000 Flash memory. You learned that the RAM sizes for the memory map range from 8 KB up to 64 KB and are available on chip. You also learned about some of the features of the External Memory Controller: it supports RAM, ROM, Flash, burst ROM, and some external I/O devices, has independent configurations of four banks, and from one to 16 programmable idle cycles. You examined the Memory Accelerator Module and looked specifically at the Pre Fetch Buffer, Data Bypass Buffer, and Branch Trail Buffer. You also examined two important Flash programming techniques, In-Application Programming and In-System Programming. Finally, you learned about some of the features of the Boot loader as well as how to protect code on the LPC2000 device.
PTM Veröffentlicht am: