Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
iMX8QXP-Slide7

SafeAssure® is one of the great features of the i.MX 8QXP as it guarantees continuous display output, even after data failures have been detected. This feature is crucial for industrial and automotive use cases in which, under no circumstance, a display can be blank. The example on this slide shows the i.MX 8QXP GPU core at its maximum capabilities showing a car cluster with full 3D graphics and a heads-up display (HUD) with a speed and turn-by-turn directions overlay. In case a data integrity error is detected or if the GPU is compromised, a failover image running in the background will be displayed automatically so critical information is always available.

PTM Veröffentlicht am: