Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
mechtronics-slide6

The next step was to use discrete logic gates to automate some of the monitoring and control functions. For example, a multi-input AND gate can be used to monitor preset temperature and pressure levels. Then if the conditions were correct, the operator would only need to press one button to activate the machine. This greatly simplifies the devices by eliminating the need to monitor the multiple gauges, operate the valves and control the pump as would be needed in an older system.

PTM Veröffentlicht am: