Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
PWM and Timer Applications Slide 11

Application notes and code examples are available for the timer use cases described in this presentation. NXP’s “lpcware.com” site is NXPs engineer to engineer community, hosting these downloadable resources as well as active discussion forums. Resources such as the LPC800 SCTimer/PWM Cookbook, and the LPC1800 Camera Interface application note are hosted on the lpcware site. Engineers can download theses and many other useful resources, and discuss ones latest application ideas on the community forums. Visit the LPCware.com site to learn more about applications of the SCTimer/PWM, and designing with NXP’s LPC line of microcontrollers.

PTM Veröffentlicht am: