Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
T1042
The T1042 QorIQ Communications Processor also combines four 64-bit e5500 Power Architecture processor cores with high-performance data path acceleration logic (DPAA), and network peripheral interfaces required for networking and telecommunications. The main difference between the T1042 and the T1040 processors is the 8-port Gigabit Ethernet Switch, which is only available in the T1040/T1020 processors.
PTM Veröffentlicht am: