Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
booting
LPC ARM microcontrollers with the SPIFI interface have two options for booting with the external SPI Flash. First, a user may set certain external pins low, which tell the MCU during start-up to look for external SPI Flash connected to SPIFI. However, if a customer wants to use those boot pins for other functions, there is an option to set a Flash bit to override the pin setting. This will free up the pins and allow the user to not worry about the dual functionality of the pins.
PTM Veröffentlicht am: