Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
if amp

IF frequency, also called Intermediate Frequency, is a frequency to which a carrier-frequency is shifted as an intermediate step in transmission or reception, for example during up/down conversion. The low noise 50 Ohm gain blocks NXP is offering, shown on the right hand side, cover IF frequencies of up to 3GHz. As mentioned previously, all listed parts are internally matched to 50 Ohm.

PTM Veröffentlicht am: