Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
UARTs Slide 2
UART stands for Universal Asynchronous Receiver/Transmitter controller which is the key component of serial communications subsystems in many applications. The UART takes parallel bytes of data and transmits them serially. At the destination, a second UART reassembles the bits into complete bytes. Serial transmission is commonly used for non-networked communication between computers, terminals and other devices. UARTs are also commonly used as interfaces for communication modules such as Bluetooth and GPRS.
PTM Veröffentlicht am: